I Would like LM3410 as two channel driver and switch between the channel externally
is it possible ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I Would like LM3410 as two channel driver and switch between the channel externally
is it possible ?
Hello Arnon,
That really depends on what your LED strings look like. Will they have about the same total forward voltage? You would need to pull DIM down while you switch between the two but if the voltages are close it should work fine. If they are much different then I guess it is still technically possible. But if you switch in a lower Vf string the output capacitor will give a surge of current through the string. In both directions you will get a transient event if they are different since the internal compensation will have to react each time. Cycling the input voltage could prevent that but it will be slower.
Regards,
Clint
The total forward voltage is very different 3 led vs 1
But only one set of the leds will be on at a time
And the off time between them can be very large (seconds)
Were will you suggest adding the external switching ?
Hello Arnon,
What is the forward voltage of the LEDs you are using and the input voltage? 1 seems pretty low for a boost converter. What kind of LED current do you need and do you require PWM or analog dimming?
In either case if the on time is low and not often and the startup time (on the order of a few ms) isn't too long you could just turn it on and off as needed. You would put an NFET between each string and the feedback pin and just enable the one you like before turn on. If it ends up you really need a buck converter they are much faster and the options improve.
Let me know and I'd be happy to make some recommendations if needed.
Regards,
Clint
Hello Arnon,
With that input voltage the LM3410 is your best choice.
Regards,
Clint
Hello Arnon,
Could you clarify what you mean by "boot strap configuration"? Do you mean run VIN from the output voltage after startup? If so you can and it would simply be a diode from both the input voltage and the output to VIN so it runs off the higher of the two.
Regards,
Clint
Hello Arnon,
That is correct, mostly. Something must have happened during the last datasheet update however as there are some missing connection points in that schematic (they appear in older datasheets). Where it says "VIN" there should be a junction between VIN, D2, and C1. There also needs to be a junction between pin 2, C3, R3, and D3.
I'm guessing they may have run some autocheck on it and the software didn't like 4 way junctions but didn't fix the connections. You still need to take into account the max VIN pin voltage and/or use a resistor and zener clamp.
Regards,
Clint