This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A91: Enable Pin

Part Number: TPS7A91

In Section 6.5 of the TPS7A91 datasheet it states that VIH(EN) is 1.1V min to 6.5V max, does that mean you can bring the EN pin higher than the power Input of the regulator? For instance, if my power Input is +1.8V can use a +3.3V signal to enable the device?