I am testing the learning cycle with a bq20z75-v160. I have completed the learning cycle successfully multiple times. MaxError drops to 1% and UpdateStatus changes to 0x06. I set the RSOCL bit in Operation Cfg C. Since setting RSOCL, I have not been able to complete a successful learning cycle. MaxError only makes it to 5% and UpdateStatus stays at 0x04. Does RSOCL prevent learning?
Kristie