Below are the voltage measured by using digital multi-meter on respective pins of BQ24610-evm with external power applied.
VCC=12.15V
PG=0V.
REGN=6V
STAT 1 -3.4V
STAT 2-3.4V
VFB=.934V
CE-3.28V
ACDRV-7.2V
BATTDRV-9.28V
BATTERY WILL POWER THE SYSTEM IF EXTERNAL POWER IS DISCONNECTED THOUGH THE SYSTEM WILL NOT CHARGE THE BATTERY.