Other Parts Discussed in Thread: BQ76920, BQ78350, BQSTUDIO
Hello All,
Help to establish the correct paraneters for bq78350-R1. I have only SMB.
I have BMS 5S bq78350-R1 V1.03 + bq76920.
Rsene 20mR - 1W, current SCD 6,65A current OCD 4,15А.
1. I set AFE Celll Map to 1F. write.
2. Send FET_EN.
3. Send RESET + Power Off
4. Set DC 21V.
5. Power ON.
6 Boot.
7 Set AOLD HEX to 5C. 320ms, 83mV, write
8 Set ASCD HEX to 8C 100uс 133mV,write.
9 Send RESET.
10 connected load 2A. Load - "ON".
BMS cut off the batteries. :( :(
11 Load off.
Why does not BMS hold the load?
Thank you
Andrew