Can I use divider resistance on EN pin to set a new UVLO? Now the UVLO is 2.2V. For example,if I want IC starts after VIN rises to 4V, can I set a 10K-pull-up and 10K-pull-down resistance on EN ?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I use divider resistance on EN pin to set a new UVLO? Now the UVLO is 2.2V. For example,if I want IC starts after VIN rises to 4V, can I set a 10K-pull-up and 10K-pull-down resistance on EN ?
Thanks!
yes, you can. But there exist some tolerance. sometimes, IC can startup even when the EN voltage is lower than 2V, like 1.7V.
Hi Hu,
Please check the following screen-shot: EN signal High minimal value is 2V, this means, when EN is higher than 2V, "all " the IC should startup. so if the customer want to make the IC startup succeessfuly, the EN signal should >=2V. But some of the IC may startup at a value low than 2V, we foudn it is 1.7V before. I'll check with the design team. if you want to control the startup precisely at Vin=4V, then extra ciruit, like the operational amplifier is needed.