Other Parts Discussed in Thread: BQ24297
Tool/software: Code Composer Studio
Hi,
I'm using bq24297 charger.
I have a problem to charge Li-po battery.
My battery size is 70mA.
But, minimum charging current of bq24297 is 100mA.
So, My battery broke down when charging by bq24927.
I think it is best to change the charger.
But now, i have to use bq24297.
Can i connect a resistor or a capacitor in a schematic diagram to make the charging current lower?
Thanks.
Best regards,
Youngjun.