This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LCD Bias Solution Promotion

Other Parts Discussed in Thread: TPS65640

Hi,

      My customer who is a LCD manufactory require a new power ic for their new LCD panel , the detail requirement is below:

VDDP=+6.2V   100mA(max)

VDDN=-6.2V   100mA(max,

VGH=18V      5mA(max)  , 

VGL=-7V       5mA(max),

VCOM=-2~0V,  1mA(max)

      Could you please introduce the suitable one for their requirement?

      Thanks !