This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27520-G4: Timeouts during gauge updating

Part Number: BQ27520-G4
Other Parts Discussed in Thread: BQSTUDIO,

Can't find any document, which specifies timeouts after those operations:

  • seal
  • unseal
  • rom mode enter
  • rom mode exit

I just found in the "Updating the bq275xx Firmware at Production" document that there should be a 250 ms delay after ROM mode exiting. But the *df.fs file (got it by reading bq27520-g4 via bqStudio) has a 4000 ms delay. So, what is the correct value?

One more question. Should I seal device after successful updating? I think, so, but diagrams in the document above doesn't show that.