Part Number: BQ27530-G1
Other Parts Discussed in Thread: BQ24161,
I am using the BQ27530-G1 together with the BQ24161 battery charger. The battery pack that is used in the device is comprised of two 18650 Li-Ion cells in parallel with a capacity of 4800 mAh and does not have a temperature sensor. I have configured the BQ27530 to use the internal temperature sensor by clearing the TEMPS bit in OpConfig register. I read in another post on this forum that to use the internal temperature sensor and detect the battery that the BI/OUT should be pulled to VCC, pin D1 on chip, with a 1.8M resistor and a 33nF capacitor to ground. Also BI/TOUT should be connected to TS with a 18.2K resistor and TS connected to ground with a 10K resistor. In this configuration the BAT_DET flag is always set, with or without the battery connected, and the fuel gauge is enabling charge CE on the BQ24161.
Is there something else that need to be configured in the BQ27530 to correctly detect when the battery is removed?
Register settings:
OpConfig = 0x6166
OpConfigB = 0x6F
OpConfigC = 0x3C
Charger Options = 0x20
Charger Reg 00 = 0x00
Charger Reg 01 = 0x00
Charger Reg 02 = 0x5C
Charger Reg 03 = 0x02
Charger Reg 04 = 0x00
Charger Reg 05 = 0x02
Charger Reg 06 = 0x00
Charger Reg 07 = 0xC8
Status:
Control Status = 0x6285
Flags = 0x0138
Application Status = 0x00
ChargerStatus = 0x00
Charger Reg0 = 0x30
Charger Reg1 = 0x30
Charger Reg2 = 0x58
Charger Reg3 = 0x8E
Charger Reg4 = 0x45
Charger Reg5 = 0xD2
Charger Reg6 = 0x00
Charger Reg7 = 0xC0