This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65912: Discrepancy in Datasheet

Part Number: TPS65912

For LDO6, Table 4-2 in the datasheet specifies a default voltage of 0.8 V for CONFIG1=0 and 1.85 V for CONFIG1=1.

However, Table 6-38 of the same datasheet specifies the default voltage for LDO6 to be 3.3 V for CONFIG1=0 and 1.85 V for CONFIG1=1.

Why is there a discrepancy for CONFIG1=0 condition and which one is the correct value?

In general, there are some serious typographical error in the datasheet that need close attention.