Part Number: TPS65912
Assuming,
- CONFIG1=0 (pin E2)
- PWRHOLD_ON (pin D6) is connected to VCC (pin H2)
- VCCS (pin G2) is connected to VCC
- SLEEP (pin G4) is connected to AGND and DGND
- VCC > 3.3 V
I'd like to know if the following two statements are correct:
- When the PMIC is powered up, it will settle in ACTIVE state.
- When the PMIC comes up in ACTIVE state for the first time, LDO7 and LDO 8 will be disabled.
Thanks!