Hi Team,
We are using two LiSOCl2 batteries in parallel. There are some questions, please help.
1. The battery is connected in parallel, but can turn on system when only have one battery.
Would this have any effect on capacity estimation when insert the second battery? How to adjust the capacity?
2. How could I configure the battery max capacity and voltage? (The battery is 1440mAh/3V)
From Tabel-1 of datasheet, The register 0x3C...0x3D is read-only.
Is this a right register to configure design-capacity and design-voltage?
(From Table 13-1 of BQ35100 Technical Reference Manual.)
3. Do I only need to do factory calibration while hardware layout change?
4. What is default mode in BQ35100?
(From Technical Reference Manual)
Thanks