This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138OL40EVM-032: Can't access to EVM, No Devices Found!

Part Number: UCD3138OL40EVM-032
Other Parts Discussed in Thread: UCD3138

Hello

we are trying to connect UCD3138OL40EVM-032 with PC. But in best cases we got next image.

We already tried next OS:

Linux Debian 8
    ccs_setup_linux64_7.2.0.00013.bin has installed
        Software by default connecting to BlackHawk LAN560 emulator 0, but we have another JTAG.
        In CCS project we can't verify Connection, no one case in list don't work.
        What should we do with it next?

    We can't found TI-Fusion-Digital-Power-Studio-3.0.20 for Linux.

Linux Debian 7

    ccs_setup_linux64_7.2.0.00013.bin hasn't installed.

    ccs_setup_linux64_6.2.0.00050.bin  has installed.
        Boot Log:

log4j:WARN No appenders could be found for logger (org.eclipse.jetty.util.log).
log4j:WARN Please initialize the log4j system properly.
dvtLogOptions.xml DOES NOT exists

       We got segmentation error when made new project.

    We can't found TI-Fusion-Digital-Power-Studio-3.0.20 for Linux.

Windows 10
    TI-Fusion-Digital-Power-Studio-3.0.20.exe has installed and working bad  - some issues in xml
    UCD3xxx Device GUI scanning devices in ROM mode and notified that it's ready for flashing, but can't found nothing in program mode.
    SMBus / I2C / SAA  tool permanently got NACK for any actions.
    Fusion Digital Studio scanning but don't found nothing - No device found, after it we can going into offline mode.
    If save Sample project for UCD31xxx and just resave with another name, then we got an error when trying to open this next project next time. Fusion Digital Studio got an error - XML with negative index.

    ccs_setup_linux64_7.2.0.00013.bin hasn't installed.
    ccs_setup_linux64_6.2.0.00050.bin has installed.
        Empty project for UCD3138 compiles with some issues, it can be fixed fixed by linker script.
        But it still not clear how to connect to EVM and how to flash devices.
        No one connection case working when we made new CCS project.

Windows 7
    TI-Fusion-Digital-Power-Studio-3.0.20.exe has installed.
    Same result as in Windows 10 - no connection, but, without crashes.

Windows Vista
    ccs_setup_linux64_6.2.0.00050.bin hasn't installed.
    Fusion Digital Studio can't found devices -  No device found,
    UCD3xxx Device GUI can found devices only in ROM mode.

How we can connect this EVM with IDE?