Other Parts Discussed in Thread: TPS563200
Hi, team.
My customer is tring to use TPS56x20x seriese devices at TV application.
Therefore, since I was asked by the customer about the function of this device,I want you to tell me.
Can you please help me?
<Question>
①-1: Please tell me about Non-latch OVP function.
In this function, when the output (target) voltage becomes 125% or more,
it is switching is temporarily stopped without latching.
my consider is OK?
①-2: Is it correct as below to distinguish existence of Non-latch OVP function from TPS 56x200 / 1/8/9 series? (If it is not correct, I'm happy if I can receive a correction comment.)
· TPS56x200/9: Switching temporarily stops due to output overvoltage detection.
· TPS56x201/8: No output overvoltage is detected and output is adjusted by fixed ON time control.
②: When considering this product by design, is there a need for a snubber circuit?
(Please tell me if it is safer to prepare the pattern even if it is not necessary,too.)
Best regards,
Masumi Sekiguchi.