Hi,
I have a problem with BQ24296M. The maximum charging current that it achive is 0.7A even if it is set to be 1.5A (by RILIM).
Could you please check if the problem is with hardware design or I set registers incorrectly?
Here go the scheme of connections:
The registers are set as below:
REG00 = 0x37,
REG01 = 0x1B,
REG02 = 0x60,
REG03 = 0x11,
REG04 = 0xB2,
REG05 = 0x8C,
REG06 = 0x73,
REG07 = 0x00,
REG08 = 0xAC,
REG09 = 0x00.
Regards.