Tool/software: WEBENCH® Design Tools
In AN SLVA412 the Design 1 is for a GSM/GPRS power supply with Vin = 8V-40V, Vout = 3.8V and Iout = 2.5A.
I'm wondering if this design is saved in Webench so I can retrieve it and do my evaluation.
thks and rgds,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
In AN SLVA412 the Design 1 is for a GSM/GPRS power supply with Vin = 8V-40V, Vout = 3.8V and Iout = 2.5A.
I'm wondering if this design is saved in Webench so I can retrieve it and do my evaluation.
thks and rgds,
That design pre-dates Webench. We did not use Webench to create it. We may have some design files remaining, but it was 7 years ago. I'll check after the holiday weekend.
Thks Arief,
but when I input similar data, Webench calculates other devices. Inductor for example I get 22uH instead of 10uH.
since I'm not expert, I'm affraid to replace devices by another one with so big difference in values and then lose efficiency, increase cost, etc..
rgds,
Agarb