Other Parts Discussed in Thread: UC1710,
Hi,
I would like to know if the TI mosfet driver UC3710DW and the UC1710J have the same die. They do not have the same package, the 1st one is SOIC and the second one is a dip but they share the same datasheet. However UC3710DW is rated for temperatures between 0°C to 70°C and UC1710J -40°C to 85°C.
Basically I would like to have a UC1710J in a SOIC package or an automotive version of the UC3710DW. Does TI have any of those?
Also can you indicate how t purchase the UC1710J from France? It is not available at any of our usual providers and it's not possible to request for samples.
Thank you for your help.
Best regards,
Annaïs