Part Number: LM3481
Hello all
There is a problem with using Lm 3841.If the problem is applied, the output load will be reduced by applying the output load after 25 V output & 2.5 A design.
I would like to keep the output current from 1.3 A to 1.5 A, but the output drops gradually due to a battery voltage drop of 8.4 volts.The output current will be 1 ampere when using several times.I want to solve this problem.