This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lp8758-E0: suitable as a power source for FPGA ?

Part Number: LP8758-E0
Other Parts Discussed in Thread: LP8758-E0

looking for powr source for FPGA

currently using 5 POWER ICEN5319QI

Vin = 5V

require following output:

1.      1.9V      <1A

2.      3.3V      <1.5A

3.      1.0V      <1A

4.      1.1V      <1A

5.      2.5V      <1A

can the LP8758-E0 handle 1, 3, 4, 5 altogether?

and chose independent buck for 2.

is the vout only configurable by communication setting?

Thanks