This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8745 80513A

Hi all. I am looking for help to cross reference an old  80's transistor with the numbers 8745 80543A . It is on a 12v DC automobile heater/ac blower motor switch circuit for variable speed control. I want to replace it with anything current instead of having to purchase the entire switch module which is very expensive since it is bmw. Thanks for any help