This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23861: if falling time of SDA and SCL is low than 20ns, which is the min value in datasheet, is there any risk?

Part Number: TPS23861


Hi

if falling time of SDA and SCL is low than 20ns, which is the min value in datasheet, is there any risk?

why TPS23861 has min time limitation?

right now, in customer's application, how to slow the falling slope?

thanks.

  • Hi Max,

    Customer needs to make sure the SCL clock frequency doesn’t exceed 400KHz and the data set-up time and hold time follow the timing spec in the datasheet.  Then the rising and falling time being lower than 20ns should not be a problem. Thanks.

    Best regards,

    Penny