This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65261-1: I have a question about implementing the TPS65261-1 function.

Part Number: TPS65261-1

Dear TI Team,

Would you help this request?

Integrate the PWM signal of the SoC as shown in the figure below and connect the signal to the DC-DC FB
Check if DC-DC output voltage control function is available.
 
-.ex) R1 : 13.3 kΩ, R2 : 27 kΩ, R3 : 69.8 kΩ, R4 : 75 kΩ, R5 : 1 kΩ, C1 : 2.2 uF, R6 option condition.