This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3890-Q1: High accuracy Reset delay

Guru 20090 points
Part Number: TPS3890-Q1
Other Parts Discussed in Thread: TPS3890

Hello,

I'm looking for a reset IC that can realize a delay time of 80 ms +/- 10 ms.
From the equation of TPS3890-Q1, we couldn't achieve 80ms +/- 10ms delay time.
Please see the attached file as my calculation based on Vdd=3.3V.
Is this calculation correct ?
Also, if there is other device which can be achieve this requirement, please let me know.
Reset Threshold is 3.3V+/-0.2V. 


TPS3890-Q1_Calculation.xlsx

Best Regards,
Ryuji