Hi everyone,
I'm using EM1402EVM (16 channels active balancing module).
- My purpose is to balancing the individual cells in the battery pack while charging.
- My battery pack is composed by 15 batteries connected in series. (Lithium Ion Prismatic Pouch Cell AMP20M1HD-A)
I install BQ76Pl455A-Q1 GUI in order connect between PC and EM1402EVM (via USB port)
- I can connect it properly and i can also see all the individual voltage.
- But when i try to balance the cell, it doesn't work as expected and it was shown as following : 
- Status of Balancing indicator light on top was RED. (means it doesn't work)
So how can i balance cells in my battery pack ? Is there any other possible way to balance?
Best regards,
TEP Pungratanak