This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24616: Absmax value of HIDRV Pin

Part Number: BQ24616

Hi Team,

I have a customer using the bq24616. During the switching of the FET on the HIDRV pin, they notice negative voltage spikes of upto -1.4V. The datasheet specifies that the HIDRV pin has a voltage AbsMax of -0.3V. Is this correct or is the HIDRV pin rated to -2V?

I'm assuming that the -0.3V vlaue is a continuous voltage and higher transients can be handled by the pin. Is this correct? Are there any limits to the transients?

Thanks and Regards,

Mihir Gupta

FAE - South Germany