Hi,
I am using the TS1..4 Pins to drive LEDs via a FET. Same circuit as on the EV Board.
If I press the LED_TOGGLE button, it Appears the pins are not pulled low and are floating between 500mV and 1V instead of being pulled low. The LEDs remain ON.
If I press the LED_TOGGLE button again, the TS Pins are pulled high to 1.74V as expected.
On the EVAL board are the 10k Thermistors on each TS Pin which act as pull-downs. I do not have them on my board.
Is there anything I do wrong or do I really need pull-down resistors to turn the LEDs off?
Thanks,
Fred