This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62095EVM-840: can't drain load over 3A

Part Number: TLV62095EVM-840

Hi,

I have test TLV62095 OCP on TLV62095EVM, but I found it can drain to 3A or higher, please see below waveform.

It define OCP by switching current right? I have plot inductor current seems maximum~ 3.064A.

That I only change R1 to 20k for set Vout to 0.9V.

CH1: Vout

CH4: IL

D822.TIF

Thanks!

Jeff