This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3489: LM3489 enable delay

Expert 4455 points
Part Number: LM3489

Hi,
I have an application where I see about 20µs enable delay (applying 5V at EN pin) until LM3489 switching on the external FET. Can you confirm there's no possibility to further reduce this enable delay.

Thanks and BR,
KF

  • Hi KF,

    In many of these converters you would see the delay to avoid unintentional glitches before the output voltage rise up . If i may know , is there a particular reason /application where you want to reduce this delay ?

    ---Ambreesh
  • I don't see any way to reduce the delay from enable the start of switching on this device.

    This device uses an external P-CH MOSFET. Many newer controllers and integrated regulators have been introduced since the release of the LM3489 product. I suggest you enter your design criteria into Webench and consider other devices that are constant frequency PWM or Constant On-time control loops. The LM3489 is an early hysteretic control loop. Much of the circuit operation is dependent on external component values and the designs are difficult to migrate from one design to the next. Because of the hysteretic control loop it is a challenge to test on the bench.