Other Parts Discussed in Thread: BQ40Z50-R1, BQ24725A, BQ4050
Hi,
We are developing a charging system and are looking for a solution to charge a LTO battery (lithium titanate) with 4 serie cells, these batteries have a low charging voltage: 2.8V and nominal voltage: 2.4V. We thought to use the bq40z50-R1 as a gas gauge for the battery and the bq24725A as charger, but we are not sure if those components are compatible whith the LTO battery requirements, is it possible to charge the battery? On other forums we read that those components are not able to balance LTO cells. If those components are not compatible, which are compatible?
Thanks!