I used TPS62737 in my program,and I have some questions abou the connections of Vin_OK and the EN pins.
The datasheet describles that EN1=0 and EN2=1 means enable buck mode,In my design,the vaue of R1,R2,and
R3 is 3.74M,1M,8.25M,which means that the voltage of VIN_OK is about 4.2V and the output is expected to be 3.3V,
However,if I connect Vin_OK with EN2,it seems that the buck mode does not work,if Idisconnect VIN_OK and EN2,
it works. I measured the voltage of Vin_OK,which seem to be 0V,whats the problem.the following is the circuit.