Hello,
I'm using BQ40z50-R1 EVM to get 4-cell individual SOC information for battery balance, and I tried to read IIii to LLll (DOD0 cell 1 to 3) in ManufacturerAccess() 0x0074 GaugeStatus2.
Therefore, I can exactly know battery capacity SOC(1-DOD) instead of voltage if battery is LiFePo4. But I noticed the value is fixed (no change) on the GUI when 4-cell battery charging ,discharging and balancing.
There are some questions :
1. Supposedly DOD0 will change when using Impedance Track™,or DOD0 is just a parameter ?
Can I use DOD0 value to determine battery capacity ?
2. If could, what's setting or condition I missing ?
3. If couldn't, do we have 4 cells individual SOC solution (like voltage,temperature)instead of totally battery pack SOC ?
4. Could I say 1-DOD = SOC ?
Please help me on this.
Thank you.
Best Regards,
Billy