This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2585: What is the baking condition for LM2585S-ADJ/NOPB ?

Part Number: LM2585

Dear Sir/Madam,

I want to check what is the baking condition for LM2585S-ADJ/NOPB with DDPAK/TO-263 (KTT) package

Based on AN-2029 Handling and Process Recommendations http://www.ti.com/lit/an/snoa550e/snoa550e.pdf Table 5, the table below only show <=4.5mm but the IC datasheet show this package height is >4.5mm. I show the forum mentioned the nominal thickness for TO-263 (KTT) is 4.445mm. Should I follow table 5 thinkness <=4.5 with MSL3 for the baking condition or you have another set of baking condition? Hope to hear from you soon.

Best regards,
Kpk