Hi,
My customer reported that they observed the error of OCD threshold is much higher than our datasheet spec. Based on datasheet, the threshold should be within 100mV+/-12.5mV, however, the measured result is arround 73.6mV, much lower than MIN spec. The voltage is measured with DVM dirrectely on SRP/SRN pins and electric load is applied on battery pack output. And also they reported that the ADC reading of the load current is fairly accurate. Bellow is the connection of SRP/SRN pins.
Thank you,
John