This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3481: Recommended circuit using shutdown

Guru 16770 points
Part Number: LM3481

Hi

I have question about LM3481.

It doesn't have enable pin, so SD pin seems to be good as alternative.

According to the datasheet, voltage of SD pin should be pulled to Vin.
Our Vin range would be between 10.8V and 26.4V.

Is it possible to apply voltage divided VIN to SD pin?
Is there considaration we should be cared?

BestRegards