Hi,
Let me talk about the Cff calculation formula.
The data sheet has the following description.
''When the output capacitor is increased to 100 μF, then the fP is reduced to 10 Hz.
Therefore, a feed-forward capacitor of 10 nF compensates for the low frequency pole.
A feed forward capacitor that sets fz-f near 10 kHz improves the load transient response in most applications,
as shown in Figure 11.''
However,
When calculating based on the following circuit example and BB,It became 54 kHz.
Is it correct with understanding that it should be set to 10 kHz or more?
Which is 10 kHz or 54 kHz correct?
Could you give me your advice?
Best Regards,
Yusuke/Japan Disty