Hello,
I am currently investigating the TPS61196 for a load driver, not an LED driver.
I have a few queries regarding the TPS61196. Please see below:
1) Is it possible to override the fault detection feature so the unit will not shut down if a fault is detected? The main fault I am having an issue with is the OVP fault.
2) Is it possible to override the soft start up sequence?
3) Is it possible to override the detection of used strings?
4) Do you see any issue with adjusting the ISET resistor with something like a Digipot for changing the current while the device is in operation?
Thank you.