The extended range datasheet has note: "In normal operation, VCC is powered through a current limiting resistor. Absolute maximum of 12 V applies when VCC is driven from a low impedance source such that ICC does not exceed 30 mA (which includes gate drive current requirement)."
Is the intent of the note to limit power dissipated in the chip? If so, is there any further information? If not, what is the intent of the note?
Thank you!