This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Universal Input Buck Controller

Other Parts Discussed in Thread: UCC28630, UCC28881, UCC25600, UCC28950

Hello everyone,


I have been searching for an high voltage DC input Buck controller with no luck. Does TI have any high voltage input Buck controller ?

I need it to be in the range of rectified mains, e.g. >325 V DC input voltage.

Thank you,

Cata

  • Hello Catalin,

    I suggest you go to the TI Designs page, click on the Power Supply tab, you'll have access to over 1,000 designs: http://www.ti.com/general/docs/refdesignsearchresults.tsp .  Click on the VIN MIN tab, sort by highest VIN.  I see two possible designs that are >320VIN.

    If these do not meet your requirements or give you a starting point, please provide more details such as VOUT and IOUT, and some additional information as to the application/what is this supply powering?

        

    ~Leonard 

  • Hi Catalin,

    Unfortunately, there is not a buck controller rated for the DC input range you are expecting. Do you know what your output requirements are? I can suggest another topology based on your requirements.

    Best Regards,
    Ben Lough
  • Hi Catalin,

    I stand corrected. Take a look at this reference design: www.ti.com/.../PMP11236

    Best Regards,
    Ben Lough
  • and another option, using WEBENCH, start with the UCC28630 ( www.ti.com/product/ucc28630 ), input your design parameters into the WEBENCH box at the right of the page and click OPEN DESIGN.

  • Thank you both.

    Sorry for giving so little specifications. I will try to improve it.

    ---Specs---

    • Input Voltage: Mains rectified voltage ~325 V DC  OR it could be the output voltage of a PFC stage with e.g. 360 VDC min and 400 VDC max and 390 VDC typical (it has to be decided, but you got the range..)
    • Output Voltage = 62 V DC
    • Output Current = 16 -17 A  (Output Power ~ 1 kW)
    • No isolation necessary because the next stage is an inverter with galvanic isolation.

    -----------------

    So, given those specs, I have some questions:

    1) Based on the topology selector page (http://www.ti.com/lsds/ti/power-management/pwm-resonant-controller-overview.page), I know Buck converter is not the suitable topology, however, is it possible to make one, even though it is not recommended ? (No isolation is necessary because the next stage of the design has galvanic isolation i.e. next stage is an inverter).

    2)  In the Power Management section -> Non isolated DC/DC Switching regulator -> Buck controller external switch (http://www.ti.com/lsds/ti/power-management/buck-controller-external-switch-products.page#), I see the highest input voltage is 100 V buck controller. They do mention output voltage and output current as well (hence, power capability).

    Ben Lough's recommendation in post #3 uses the UCC28881 controller with integrated MOSFET. It specifies the output current capability since it has a MOSFET built it. However, what I do not understand is that in the UCC28630, it does not have an integrated MOSFET, does not have any current specifications, but in the datasheet they do specify that it has a 60W output power (max). So my question is, why do they specify that, even though the controller does not even play a role in the power stage, meaning, it is not in the power path, has nothing integrated which would be in the power path ?

    Is it only a recommendation ? Can 1 kW Buck converter be built with that controller (even though it is not the best solution) ? PD: I have used the WebBench designer tool but no design is available since it can not find a MOSFET to handle the current. I will figure out the MOSFET, I only care whether the controller chip will catch fire or not.

    3) In my opinion, for 1 kW, the best SMPS topology would be between LLC , Full Bridge and Phase Shifted Full Bridge, do you agree ? If you do not agree, can you recommend what is the suitable topology for this case?

    4) Can you recommend an IC controller for a topology given in question 3).

    5) 1st page of the datasheet of UCC25600 says it is intended for 100W to 1 kW PSU, trying to build one for 1 kW would be too close to its maximum margin, or could be fine ?

    Thank you very much for answering and wasting your time with me even though I was not clear from the very beginning.

    Best regards,

    Cata

  • Cata,

    UCC28950 as phase shifted full bridge is probaby your best option. That can essentially be used as a buck. You may still want to use a transformer for step down help. THis is ZVS controller for highest efficiency and a very popular device with proven history.

    Regards,
    John