This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: Max delay time setting on UCC28950

Part Number: UCC28950


Hello Team,

As per datasheet, maximum allowable resistor value for RAB, RCD, REF is 90kohm.

Which implied maximum delay time of 1.7uS.

Is there a way to increase this delay time further?

If not, what care needs to be taken in design so that dead time requirement is much lesser than 1.7uS?

Regards,

Mahendra

  • Hi Mahendra,

    The engineer who supports the UCC28950 is OOO today but you should see a response tomorrow to this post.

    Regards

    Peter
  • Hi Mahendra

    I'm sorry but 90k Ohms is the max allowed resistor. Normally 1.7us is an adequate delay maximum and I'm not aware of any instance where it has proven to be too short.
    The dead time should be slightly longer than the time needed for the switched nodes to swing from Vin to GND and vice versa - the time is difficult to calculate directly because it depends on stray capacitances in the physical hardware and to some extent on propagation delays in the driving circuitry.
    Do you have a specific reason for thinking that you may need longer ?

    Regards
    Colin