This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3407: About maximum value of RISNS

Guru 21045 points
Part Number: LM3407


Hi Team,

 

Our customer would like to use LM3407 at the following conditions so they have to use RISNS =around 2.475ohm.

Can I use this RISNS?

If no, could you please let us know the maximum value of RISNS?

 

[Conditions]

-VIN=10V to 20V

-VOUT= around 6V

-ILED=around 80mA (1 LED)

 

Regards,

Kanemaru