This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: BQ76940 / BQ78350-R1 Timing 250ms Tolerance

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQ76940,

Hi all,

We are using BQ76940 / BQ78350-R1, reading out Data via SMBUS with a uC triggered by Alert  and giving then Data via Uart to a Subsystem.

This Subsystem needs the Data in a Range between 250-260ms.

As far as we undertsandm, the timing is given by System Scheduler in the Frontend.

So we found some cases where the timer was near 240ms.

Can someone from TI please give us the possible range/tolerance  for the Scheduler ?

Thank you