Hi,
I want to use a TPS65800 to power a datalogger.
Inputs are to different 5V sources.
As Outputs I need :
5V 200mA
3,3V 50mA (for ADC)
3,3V 300mA
I thougt I could use the internal regulators of the TPS to generate the two 3,3V supplies. But as I want to use an LiPo with its minimum voltage of 2,5V the internal regulators of the TPS wouldn't work. So I thougt to boost the outputvoltage of the TPS (2,5 to 4,2V) to 5V and feed it into the internal regulators of the TPS. Is this possible? or how I could create 3,3V with the TPS , with only 2,5V available from the lipo.
Thanks for you help
best regards Simon