Can the slew rate of the TPS22810 be adjusted to values much longer than shown in the datasheet risetime table 2? The longest values there are around 8 ns.at 18 V.
In my application I need to slew 0 to 15 V in no less than 100 ms. If the TPS22810 is not the right device for this, is there a TI part that is?
Whit