This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: Assistance for BMS of a battery pack

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQ76940, , BQ78350, BQ76200

Hello all,

A customer ask,

" We need assistance for a BMS of a 11S1P battery pack where the BQ78350-R1 and BQ76940 are used.
1. When Cell UnderVoltage flag (CUV) is set, the battery seems to distort the following I²C transaction. as soon as this bit is cleared (e.g. we set the CellUndervoltageRecoveryThreshold to a lower value) the I²C bus does work. Something inside BQ78350 behaves different when this flag is set - what and why???
2. We modified the RSOC TerminateCharge (TC) Thresholds to 85% (clear) and 90% (set) - why does it disable the charge mosfet when charging is interrupted a short time. Although CellOverVoltage (COV) threshold is not reached and battery should still be able to be charged. Isn't the RSOC calculation only used for indication - not for safety protections?? Can we disable that? An untrained battery may have an RSOC of anything, but should still be able to charge until the charger circuit determines the CCCV & Timing end condition."


Could anyone help me with this please?

Thank you in advance.