Part Number: LM2703
Hello Team!
Could you help please.
My customer have question about LM2703:
In their devices they are using LM2703
Vin = 2.4 to 5V, Vout = 7.2V, I_load = 20 - 30mA continuous (max).
As diode(datasheet's figure 6.) they used BAS316(NXP/Nexperia). But now it is discontinued. And they are looking for replacement.
In datasheet described it should have Switch current limit from 260 to 400mA.
BAS316 has continious forward current - 250mA(max).
So there are questions:
1)This way with BAS316 the circuit works more than 10years without faults. How is it possible?
2)Which I_load is the maximum for the LM2703 with diode like BAS316?
They have 2 replacemnts from ONS: BAS16HT1G and MMDL914T1G. But their continuous forward current is lower = 200mA(max), repetitive peak forward current) = 500 mA (max).
Can they use one of this diodes with LM2703?
In LM2703's datasheet described it should have diode like MBRM130LT1 with continuous forward current) = 1 A (max), IFRM (repetitive peak forward current) = 2 A (max).
Can they use variants with lower parameters?
Thank you in advance!