Other Parts Discussed in Thread: TPS62125, TPS62745
For a new product we tested the TPS78001 where the EN pin is used to switch the device on and off, in this case we make use of the hysteresis of the EN pin.
Its datasheet mentioned on page4 that the input has logic levels, but on page11 of its datasheet (figure 35) also the real levels are specified as function of the temperature.
In our application the input supply voltage of the TPS78001 is fed to the EN pin via high-ohmic resistors, which works very well.
Now we consider to use the TPS62740 for better efficiency, it seems to have similar input characteristics on the EN pin, but its datasheet is only mentioning the logic levels.
Can you confirm/specify the actual hysteresis levels also for the TPS62740?