Captured to TPS65023 Disable PFM mode wiki page

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65023; PFM mode, extra capacitance

Other Parts Discussed in Thread: TPS65023

When the TPS65023 opreates with light loads (<10mA) on DCDC3, does increasing output capacitance force converter into PWM mode, reducing overall ripple voltage?

  • 2. For light loads (<10mA) the DCDC converter will not operate in PWM mode by adding additional output capacitance.

        The decision if the converter operates in PWM or PFM mode is done on the average inductor current.

         Please have a look at equations (1) and (2) on page 22 of the TPS65023 datsheet.

        You can simply force the converter in PWM mode by I2C command.

        On the othe hand you can not increase the output capacitance without  limit, this will cause instability of the converter.