This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50EVM-561: no change in the RSOC while attempting to charge

Part Number: BQ40Z50EVM-561
Other Parts Discussed in Thread: BQSTUDIO, BQ4050EVM-561

Hello,

I am attempting to test the BQ40z50evm-561 using the BQ studio. I am attempting to run a charge and discharge simulation. I have connected the Pack+ and the Pack- to the charger. I have removed the SYS PRES to Pack- wire as i have set the NR bit in the DF configuration. I first attempted to charge the battery pack by FET_EN=1. Since that process did not work i continued by setting CHG_TEST=1 and DSG_TEST=1. This also did not charge my battery pack. The pack i am testing (INR18650-30Q) came with a stock fuel-gauge and so ran another test by attempting to charge the pack through their connection but still attempting to read the bq40z50EVM. As the pack charged the RSOC did not change from 16% nor did the remaining capacity change as the battery voltage continued to rise.

If anyone has any idea as to why this kind of issue is happening, i would appreciate the help

Thank You,

Steven