Part Number: TPS56221
Hi all,
I'm trying to use the TPS56221 to create a 12V in, 5V 18A output application, but I'm getting a bit confused looking at the example provided in the datasheet. www.ti.com/.../tps56221.pdf
1. Why in section 8.2.2 R1 is listed as 1.78kOhm, but then in 8.2.2.11 it is listed as 2.83 kOhm ?
2. In Table 1 in section 8.2.1 what is Itran ? Is it always 10A or is that up to the user?
3. In Table 1 in section 8.2.1 Iout(max) is 25A, but then in section 8.2.2.4 equation 10 uses Iout(max) = 30A (equation 9 uses 25A...), and then again in section 8.2.2.11 Iout(max) = 30A, where is this 30A coming from and why are they not using 25A throughout their calculations??
Thanks in advance!